Trade Press Releases for SPS & electronica

Trade Press Releases for SPS & electronica

Welcome

Here you will find the latest trade press releases of the Weidmüller Group regarding the SPS 2024 fair in Nuremberg, Germany and the electronica 2024 fair in Munich. All articles and images are freely available to you. We would be pleased to receive a copyright notice.

u-mation | Hardware for Industrial IoT & Automation

I/O System u-remote

Weidmüller, a leading provider of products and solutions for electrical connections and automation technology, announces the market launch of its latest power measurement modules for the u-remote I/O system. The four modules offer precise measurements, higher accuracy and seamless integration into existing automation systems. 

Download Press Release

Switches

Weidmüller is introducing a new unmanaged switch with Single Pair Ethernet (SPE) connection. The switches raise the performance of industrial applications to a new level. The SPE technology increases the range of the internet connection and at the same time the two-wire cables enable parallel power transmission.

Download Press Release

u-software | Software for Industrial IoT & Automation

u-OS Data Hub

Weidmüller is expanding the u-OS operating system with the Data Hub. The Data Hub networks different applications installed on u-OS with one another. This makes it easier for users to make use of variables and make variables from one application visible to another.

Download Press Release

PROCON-Connect

Weidmüller launches the PROCON-Connect App. The software tool enables users to easily capture machine data, pre-process it and make it available to other applications. This simplifies data exchange and speeds up installation.

Download Press Release

Machine Learning at the edge

The new edgeML machine learning solution from Weidmüller works independently of cloud and internet access. Learning algorithms can now run directly at the edge – whether in the form of a PLC or IPC. Moreover, the software is available as a Docker container. This means that edgeML is manufacturer-independent and can be used on all standard industrial controllers that support the execution of Docker containers.

Download Press Release

Energy Management in Accordance with ISO 50006 – Regression Analysis

Regression and correlation analysis for the ResMa® energy management system expands possibilities for energy managers. The supplementary tool scrubs data and harmonises KPIs. With the expansion module, companies can operate their energy management systems in accordance with ISO 50006 and meet the specifications of the EU corporate sustainability reporting guidelines (CSRD).

Download Press Release

Partnerships

Fortinet

At the Smart Production Solutions (SPS) trade fair, Weidmüller, a pioneer in industrial connectivity and electronics, announced a strategic partnership with Fortinet, one of the global cybersecurity leaders driving the convergence of networking and security, that will provide robust cybersecurity competencies for operational technology (OT) environments. The collaboration targets the emerging need for strong cybersecurity due to increasing IT and OT convergence – the trend structurally changing the face of industries worldwide.

Download Press Release

Orange Cyberdefense

The French company Orange Cyberdefense and Weidmüller, the international specialist for electronics and connection technology based in Detmold, Germany, announced their strategic partnership in the field of cybersecurity consulting at the Smart Production Solutions (SPS) 2024 trade fair. The aim of the collaboration is to provide manufacturing companies with easier access to comprehensive cybersecurity consulting services.

Download Press Release

TÜV Nord

Weidmüller has received the certificate for industrial IT security according to IEC 62443-4-1 from TÜV Nord. IEC 62443 is the most important internationally recognised standard for IT security in automation and control systems. The certificate underlines Weidmüller's commitment to developing secure-by-design products. The aim is to enable customers to operate their machines and systems safely with secure-by-design products and to comply with legal security requirements such as the NIS2 Directive and the Cyber Resilience Act (CRA).

Download Press Release

Eplan

Fast, simple and intuitive labelling and assembly of components in panel building with Eplan Smart Mounting and Weidmüller’s LPC

Together, the digital assembly assistant Smart Mounting from Eplan and Weidmüller’s LPC make it possible to combine intuitive workflows for everything from the planning phase to the shopfloor in a new way.

Download Press Release

Connection Technologies

SNAP IN

With SNAP IN, the electronics and connectivity company Weidmüller introduced innovative connection technology in 2021, which is already setting new standards in the field of connectivity – and is also optimised for panel building of the future. SNAP IN enables automated wiring by industrial robots.

Download Press Release

Klippon® RailSnapper

Just click fully equipped DIN rails directly on the mounting plate

The Klippon® RailSnapper allows the full utilisation of the entire rail length. The entire length of the rail can be fitted with components and then pressed directly onto the mounting plate and installed in the assembly hall.

Download Press Release

Field Wiring

Networking automation and control technology is an important aspect of wiring in the field, or field wiring. At the highest technical level, this is a smart system for transmitting controller and sensor data in industrial applications. In addition, it serves as the backbone of modern industrial networks, which include almost all aspects of a production facility or process control system. As a comprehensive solution, it offers the option of connecting and integrating all electrical and electronic components – from sensors to actuators, control units or communication devices.

Download Press Release

Easy and efficient: the Weidmüller ConnectorGuide

The search for the right PCB connection technology for different device applications is often a time-consuming and tedious task. With the ConnectorGuide, Weidmüller has added a product to its portfolio that offers device developers two simple functions for finding customised solutions – and ordering free samples of them directly.

Download Press Release

Single Pair Ethernet

Single Pair Ethernet as key technology

By reducing data transmission to a single twisted pair of wires, Single Pair Ethernet (SPE) marks a major advance in Ethernet technology. This innovation not only allows high data transmission rates over longer distances, but also supports multi-drop networks and simultaneous power supply using the same cable. These features make SPE particularly advantageous in applications where cost efficiency and the conservation of space and weight are top priorities, making it an ideal solution for industrial and commercial applications.

Download Press Release

Single Pair Ethernet – applications in data communication

Increasing industrial automation requires sensor and actuator landscapes of ever greater complexity which must be integrated into efficient and scalable communication networks. Single Pair Ethernet (SPE) plays a key role here, as it enables end-to-end Ethernet communication from the enterprise level to the sensor and actuator level. One decisive advantage of SPE is its ability to bridge large distances of up to 1,000 metres without additional gateways. In addition, the integration of Power over Data Line (PoDL) enables SPE to transmit both data and energy via a single wire pair. These properties make SPE a pioneering technology for the next generation of industrial automation in the context of the Industrial Internet of Things (IIoT).

Download Press Release

Weidmüller supports the standardisation of Single Pair Ethernet

By agreeing on a standardised connector face for Single Pair Ethernet, the industry is now taking a decisive step towards the future. The new SPE connector system offers a standardised mating face for applications in the control cabinet, in the field and also for hybrid installations.

Download Press Release

Consulting

Connectivity Consulting

Weidmüller Connectivity Consulting makes processes at AuCom MCS GmbH & Co. KG. faster and more efficient

The manufacturer of electronic drive technology from Germany’s Münsterland region becomes the most important location within the AuCom Group

Download Press Release

Surge Protection

Varitector AC BS60 – Surge protection for 60 mm busbar systems

Powerful lightning and surge protection is crucial to ensure system availability in buildings, industrial plants and power plants. The components protect increasingly sensitive infrastructures from costly failures and, in many areas, are even mandatory. With the VARITECTOR AC BS60, Weidmüller has expanded its portfolio to include lightning and surge protection components for 60 mm busbar systems.

Download Press Release

Energy Solutions

DC Innovation Hub at the Weidmüller Academy

Weidmüller is setting a forward-thinking standard with its new DC Innovation Hub in Detmold, designed to bridge technological innovation and hands-on training. The DC Innovation Hub is aimed equally at customers, users, and partners, providing a space where they can explore and test direct current technologies through pilot projects. This hub impresses with its holistic approach: Weidmüller integrates applications, products, innovations, and training solutions, creating a seamless transition from technology to practical use in everyday working life.

Download Press Release